Powered by phenomenal rise in mobile penetration, data and broadband services and riding high on demand for Cloud Services, India is a growing market for CoLocationDatacenters.Gartner predicts the colocation and hosting market in India will be worth $1.3bn by 2016. It is an emerging trend in multiple sectors with Banks and Government being two major sectors fuelling CoLocationDatacenter growth in India. While the upswing in demand provides unmatched opportunities to CoLo enterprises, the competition for the fast crowding market space is getting more intense. It is no more enough to offer price differential alone; clients are now demanding value beyond the proverbial dollar.
Factors driving DCIM growth in CoLocation data centers
Data Center Infrastructure Management (DCIM) Solutions are now providing CoLo managers opportunities to build differentiation. CoLo managers are challenged to deliver cost advantage while providing holistic managed services to their clients including real time reporting, risk alerts and flexibility to upscale or downscale operations, which can be addressed by choosing the right DCIM solution. The Indian DCIM market has grown over 300% in past 5 years – from INR 150 crore to nearly INR 500 crore in 2015. Sectors like BFSI, government, IT/Telecom and Ecommerce will add further to this accelerated growth. However, most players in the market providing standardized services, are making it difficult to choose the right DCIM solution for optimal advantage.
Here are the top considerations for the CoLo Managers to choose the right DCIM for their operations:
Looking beyond the obvious benefits / The ROI for businesses
Colocation facilitates organizations to derive benefit from faster networking and resilient connectivity at a considerable cost. In such an environment, the organisations have full control over their own assets thereby increasing their business potential. A colocation offers diverse opportunities providing organizations with added levels of risk management and the chance to invest in better equipment and state-of-the-art servers. And to top it up, DCIM solutions deployed within a CoLocationDatacenter allow the organizations to align their IT infrastructure to the business objectives and enable them to optimize ROI.
System-generated reports provide visibility into racks showing the details exactly what devices they own and where they are located in the data center. It helps them upscale or downscale accordingly, without impacting running applications and providing them with ready insights to plan for future infrastructure updates. All these together ensure optimal equipment utilization.
Besides, DCIM helps in optimizing power and energy consumption. An ideal DCIM solution will provide granular data on power consumption pattern of each equipment in a CoLocationDatacenter at any point of time enabling the organization to pre-empt any excess or sudden drop.
The right DCIM solution offers all its customers within a colocation access to real time data along with the convenience of offshore monitoring.
In short, DCIM allows organizations the flexibility of using a shared datacenter while retaining real time visibility and operational management of their assets, networking and energy utlilization.